:SOURce:LIST:RDC[:STATe] {ON|OFF|1|0}
:SOURce:LIST:RDC[:DATA]?
This command sets/gets Rdc measurement. This setting is retained even if the active table is changed.
|
Parameter |
State |
|
Description |
Sets/gets Rdc measurement |
|
Data type |
Boolean |
|
Range |
ON or 1: Instructs instrument to perform Rdc measurement (turns on Rdc measurement function) OFF or 0: Instructs instrument to NOT perform Rdc measurement (turns off Rdc measurement function) |
|
Preset value |
OFF or 0 |
{1|0}<newline><^END>
Meas Setup > Rdc Meas > ON|OFF