:SOURce:LIST:RDC:OFSCancel {ON|OFF|1|0}
:SOURce:LIST:RDC:OFSCancel?
This command turns ON/OFF the offset cancel function for the Rdc measurement.
The offset cancel function allows you to eliminate offset measurement error (the measured Rdc value when the measurement signal is not applied) during measurement that occurs when dc current is superposed on the measurement cable used for measurement.
When the offset cancel function is ON, the Rdc measurement is performed in 2 ways, that is, with the measurement signal applied and not applied. After that, the measured value is calculated based on the value obtained by subtracting the measured value when the signal is not applied from the one when the signal is applied.
To use the offset cancel function, turn ON the offset cancel function before measuring calibration/compensation data.
|
Parameter |
State |
|
Description |
Turns ON/OFF the offset cancel function for Rdc measurement |
|
Data type |
Boolean |
|
Range |
ON or 1: Turns ON the offset cancel function OFF or 0: Turns OFF the offset cancel function |
|
Preset value |
OFF or 0 |
{1|0}<newline><^END>
No equivalent key is available on the front panel.