:SOURce:LIST:SWEep:LOGarithm <nop>,<freq start>,<freq stop>,<ave>,<osc lvl start>,[<osc lvl stop>]
Sets up the active table by specifying the start/stop frequency values, averaging factor, and start/stop oscillator levels. Frequency values are expanded logarithmically. This command generates the same table as the Quick Edit. Oscillator levels are always expanded linearly. Use the :SOUR:UNIT command to select the unit for the setting.
|
Parameter |
<nop> |
<freq start> |
<freq stop> |
|
Description |
Number of measurement points |
Start value of frequency |
Stop value of frequency |
|
Data type |
Integer |
Real |
Real |
|
Range |
1 to 201 |
1E6 to 3000E6 |
1E6 to 3000E6 |
|
Resolution |
1 |
1E3 |
1E3 |
|
Parameter |
<ave> |
<osc lvl start> |
<osc lvl stop> |
|
Description |
Averaging factor |
Start value of the oscillator level |
Stop value of the oscillator level.*1 |
|
Data type |
Integer |
Real |
Real |
|
Range |
1 to 100 |
Depends on the unit |
Depends on the unit |
|
Resolution |
1 |
Depends on the unit |
Depends on the unit |
*1 Default value is the same as the <osc lvl start>
Stim Table > Quick Edit