:SOURce:LIST:TABLe <numeric>
:SOURce:LIST:TABLe?
This command specifies which table to use as the active table.
|
Parameter |
Value |
|
Description |
Number of the table that should be the active table |
|
Data type |
Long integer type (Long) |
|
Range |
1 to 8 |
|
Preset value |
1 |
|
Resolution |
1 |
If your specified parameter is beyond the valid range, the instrument ignores the parameter and uses either the maximum or minimum value depending on whether the parameter is greater than the upper limit or smaller than the lower limit.
{numeric}<newline><^END>
No equivalent key is available on the front panel.