:SYST:PERS:MOD

Type

Command/Query

Syntax

:SYSTem:PERSona:MODel[:DATA] <string>

:SYSTem:PERSona:MODel[:DATA]?

Description

This command changes its model number of IDN string to the specified value. The string cannot include comma. (if comma is specified, it will be replaced with space) The empty string or :SYST:PERS:MOD:DEF reverts it to the default. This setting should be retained after power cycle.

Variable

Parameter

string

Description

Model number

Data Type

Character string type (String)

Range

256 characters

Preset Value

E4982A

Query Response

<string><newline><^END>

Examples

Dim Var as String
Var = "E1234A"
Ena.WriteString ":SYST:PERS:MOD " & Var, True
Ena.WriteString ":SYST:PERS:MOD?", True
Var=Ena.ReadString

Related Commands

*IDN

:SYST:PERS:MAN

:SYST:PERS:MOD:DEF

Equivalent Softkey

None

COM Command Syntax (Internal Control Only)

SCPI.SYSTEM.PERSONA:MODEL:DATA