Command/Query
:SYSTem:TIME <hour>,<min>,<sec>
:SYSTem:TIME?
This command sets/gets the time of the clock built in the E4982A. When you logged in the E4982A as standard user, an error occurs. Log in the user name of "Administrator" is required in case of Windows 10.
|
Parameter |
<hour> |
<min> |
<sec> |
|
Description |
Hour part of the time (in 24-hour format) |
Minute part of the time |
Seconds part of the time |
|
Data type |
Long integer type (Long) |
Long integer type (Long) |
Long integer type (Long) |
|
Range |
0 to 23 |
0 to 59 |
0 to 59 |
|
Resolution |
1 |
1 |
1 |
If your specified parameter is beyond the valid range, the command fails and an error is generated.
{hour},{min},{sec}<newline><^END>
System > Misc Setup > Clock Setup > Set Data and Time...
SCPI.SYSTEM.TIME