:TRIGger:SLOPe {POSitive|NEGative}
:TRIGger:SLOPe?
This command sets/gets the polarity of the external trigger signal input through the rear panel EXT TRIGGER terminal and the handler interface.
|
Parameter |
String |
|
Description |
Polarity of external trigger signal input |
|
Data type |
String |
|
Range |
POSitive: Positive (triggering at the rising edge from the LOW level to the HIGH level) NEGative: Negative (triggering at the falling edge from the HIGH level to the LOW level) |
{POS|NEG}<newline><^END>
Trigger Mode > Ext Trig Polarity > Positive|Negative