Performing Statistical Analysis

To perform statistical analysis and retrieve the results, use the following command:

The command shown above returns the statistics based on the measurement results at the measurement point(s) specified for each specific measurement item. The statistics include the following 10 items:

    1. Average

    2. Standard deviation σ

    3. 3×σ/average

    4. Minimum value

    5. Maximum value

    1. Number of successful measurements (number of samples used for statistical analysis)

    2. Number of measurements that were detected to exceed the Rdc limit range

    3. Number of measurements that were detected to show an overload

    4. Number of measurements that were detected as either exceeding the Rdc limit range or showing an overload or both.

    5. Total number of measurements

You can perform statistical analysis only on those measurement items that are currently displayed on screen with their underlying measurement data stored in memory. These items can include the following:

Sample Program

See the Statistical Analysis.

Other topics about Statistical Analysis of Measurement Results