The E4982A can be controlled by an external controller through the GPIB (General Purpose Interface Bus) interface. The following procedure is used for checking and editing the GPIB address.
Press System to activate the softkey menu.

To edit the GPIB address, continue with the following steps.
Click GPIB Address.
Use the numeric keys in the ENTRY block to enter the new GPIB address.
The GPIB address can be set using whole numbers from 0 to 30.