The three function keys on the front panel offer quicker, one button access to softkeys that are often used.
The default settings are as follows:
F1 key - Capture Image
F2 key - File Utility
F3 key - Toggle beep warning
Follow the procedure below to change the setting of the function keys.
Press System to activate the softkey menu.
Click Misc Setup.
Click F1 Key|F2 Key|F3 Key.
Click Capture Image|File Utility|Toggle Beeper Warning|Save State File|Save AutoRec.sta|Recall AutoRec.sta|Toggle Window Normal/Max|Toggle Window Min/Max|Telnet localhost.