:CALC<Ch>:PAR<Tr>:SEL

Type

Command

Syntax

:CALCulate<Ch>:PARameter<Tr>:SELect

Description

This command sets the selected trace as active trace. Use :DISP:WIND:ACT to activate the channel.

Examples

Ana.WriteString ":CALC1:PAR1:SEL", True

Related Commands

:CALC:PAR:COUN

:DISP:WIND:ACT

Equivalent Softkey

Trace Next, Trace Prev

COM Command Syntax (Internal Control Only)

SCPI.CALCULATE(Ch).PARAMETER(Tr).SELECT

 

 

For :CALCulate<Ch>[:SELected]:xxxx commands, we have another expression of CALCulate<Ch>:TRACe<Tr>:xxxxxx. The trace number can be selected at the same time.

 

For example:

:CALCulate1:PARameter2:SELect

:CALCulate1:AVER

 

The same operation can be done by:

:CALCulate1:TRACe2:AVER