*IDN

Type

Query

Syntax

*IDN?

Description

This command reads the product information (manufacturer, model number, serial number, and firmware revision number) of the E4990A.

Variable

Query Response

{string 1},{string 2},{string 3},{string 4}<newline><^END>

Examples

Dim Var as String
Ana.WriteString "*IDN?", True
Var=Ana.ReadString

Related Commands

*OPT

Equivalent Softkey

System > Firmware Revision

COM Command Syntax (Internal Control Only)

SCPI.IEEE4882.IDN