Query
*LRN?
This command gets the device setup query. This command is defined as "Learn Device Setup Query" in IEEE 488.2. The command returns instrument settings by binary block data (same as Save/Recall state file contents) with "SYSTem:SET " prefix.
The returned data is the same as the contents of state file which can be saved by the :MMEM:STOR. Therefore, the returned data contents is changed according to the setting of :MMEM:STOR:STYP.
{binary}<newline><^END>
Dim LRNData() As Byte, SETData() As Byte, NoofByte As Double
'*** Get the LRN data as Binary data
Ana.WriteString "*LRN?", True
LRNData = Ana.ReadIEEEBlock(BinaryType_UI1, False, True)
'*** Save the LRN data in the file
Open "C:\LRN.dat" For Binary As #1
Put #1, , LRNData()
Close
MsgBox "Get Data"
'*** Recall the LRN data from the file
Open "C:\LRN.dat" For Binary As #1
NoofByte = LOF(1)
ReDim SETData(NoofByte)
Get #1, , SETData()
Close
'*** Send the LRN data to E4990A
Ana.IO.Write SETData, NoofByte
No equivalent key is available on the front panel.
SCPI.IEEE4882.LRN