*TST

Type

Query

Syntax

*TST?

Description

This command is self-test query. The self-test is not executed by this command in the case of the E4990A. Always returns 0 for IEEE compliance.

Variable

Query Response

{0}<newline><^END>

Examples

Dim Var as Integer
Ana.WriteString "*TST?", True
Var=Ana.ReadNumber

Equivalent Softkey

No equivalent key is available on the front panel.

COM Command Syntax (Internal Control Only)

SCPI.IEEE4882.TST