Command
:MMEMory:STORe:TRACe <Value>, {TRACe|CHANnel|DISPlayed}
This command saves the formatted data array for the traces into a file in the CSV format (extension ".csv"). This command is available at revision A.2.10 and above.
Specify the file name with the extension. When you use directory names and file name, separate them with "\" (back slash), or "/" (slash).
|
Parameter |
Value |
|
Description |
File name in which you want to save the formatted data array (extension ".csv") |
|
Data Type |
Character string type (String) |
|
Range |
254 chars |
|
Parameter |
Selection Option |
|
Description |
Target traces for save |
|
Data Type |
Character string type (String) |
|
Range |
TRACe: Active trace only (This is the same as :MMEM:STOR:FDAT) CHANnel: All traces in the active channel DISPlayed: All displayed traces in displayed channels |
|
Preset Value |
TRACe |
Dim Var as String
Var = "D:\data1.csv"
Ana.WriteString ":MMEM:STOR:FDAT " & Var & ", CHAN", True
Save/Recall > Save Trace Data...
SCPI.MMEMORY.STORE.TRACE