:MMEM:TRAN

Type

Command/Query

Syntax

:MMEMory:TRANsfer <Value>

Description

This command transfers data (file) between the built-in storage device of the E4990A and external PC through SCPI command, but not through COM command.

      • When you use directory names and file name, separate them with "/" (slash) or "\" (backslash). If a file with the specified file name already exists for writing or if the specified file does not exist for reading out (Query), an error occurs and the command is ignored.

Variable

Parameter

Value

Description

File name on the built-in storage device

Data Type

Character string type (String)

Range

254 chars

 

Query Response

{Byte}<newline><^END>

Examples

See Transferring Files.

Equivalent Softkey

No equivalent key is available on the front panel.

COM Command Syntax (Internal Control Only)

SCPI.MMEMORY.TRANSFER