:SENS<Ch>:CORR2:ZME:LOAD:POIN

Type

Query

Syntax

:SENSe<Ch>:CORRection2:ZMEas:LOAD:POINts?

Description

This command returns the number of points of frequency stimulus array of Load for the fixture compensation. SENS:CORR1:ZME:LOAD:POIN causes an undefined header error.

Query Response

{numeric}<newline><^END>

Examples

Dim Var as Long
Ana.WriteString ":SENS1:CORR2:ZME:LOAD:POIN?", True
Var=Ana.ReadNumber

Related Commands

:SENS:CORR:ZME:LOAD:FREQ

Equivalent Softkey

No equivalent key is available on the front panel.

COM Command Syntax (Internal Control Only)

SCPI.SENSE(Ch).CORRECTION(2).ZMEAS.LOAD.POINTS