Command/Query
:SENSe<Ch>:CORRection<Type>:ZMEas:OPEN[:DATA] <Value>
:SENSe<Ch>:CORRection<Type>:ZMEas:OPEN[:DATA]?
This command gets the actual impedance array of the open standard for the fixture compensation. <type>: User calibration=1, Fixture Compensation=2
The array size (number of point):
User calibration: 2 × (value returned by :SENS:CORR:ZME:POIN)
Fixture compensation: 2 × (value returned by :SENS:CORR:ZME:OPEN:POIN)
|
Parameter |
Value |
|
Description |
Open standard impedance array
Where n is an integer between 1 and NOP (number of measurement points): <numeric n×2-1>: Real part of data (complex number) at the n-th measurement point. <numeric n×2>: Imaginary part of data (complex number) at the n-th measurement point. The number of data is {NOP×2} |
|
Data Type |
Variant type Array (Range) |
{numeric 1}, .... ,{numeric NOP×2}<newline><^END>
No equivalent key is available on the front panel.
SCPI.SENSE(Ch).CORRECTION(2).ZMEAS.OPEN.DATA