:SOUR<Ch>:ALC:TOL

Type

Command/Query

Syntax

:SOURce<Ch>:ALC:TOLerance <Value>

:SOURce<Ch>:ALC:TOLerance?

Description

This command sets/gets the ALC target %.

Variable

Parameter

Value

Description

Tolerance value

Data Type

Numeric type (Real)

Range

0.05 ~ 10

Preset Value

5

Unit

%

Resolution

-

Query Response

{numeric}<newline><^END>

Examples

Dim Var as Double
Var= 0.1
Ana.WriteString ":SOUR1:ALC:TOL " & Str(Var), True
Ana.WriteString ":SOUR1:ALC:TOL?", True
Var=Ana.ReadNumber

Related Commands

:SOUR:ALC

:SOUR:ALC:COUN

Equivalent Softkey

Sweep Setup > OSC Level > ALC > Target %

COM Command Syntax (Internal Control Only)

SCPI.SOURCE(Ch).ALC.TOLERANCE