:SOUR<Ch>:BIAS:DEL

Type

Command/Query

Syntax

:SOURce<Ch>:BIAS:DELay <Value>

:SOURce<Ch>:BIAS:DELay?

Description

This command sets/gets wait time after DC bias setup

Variable

Parameter

Value

Description

Delay

Data Type

Numeric type (Real)

Range

0 ~ 30

Preset Value

0

Unit

s

Resolution

1m

Query Response

{numeric}<newline><^END>

Examples

Dim Var as Double
Var= 0.01
Ana.WriteString ":SOUR1:BIAS:DEL " & Str(Var), True
Ana.WriteString ":SOUR1:BIAS:DEL?", True
Var=Ana.ReadNumber

Related Commands

:SOUR:BIAS:STAT

Equivalent Softkey

Sweep Setup > DC Bias > DC Bias Delay

COM Command Syntax (Internal Control Only)

SCPI.SOURCE(Ch).BIAS.DELAY