Command/Query
:SYSTem:TIME <Value1>, <Value2>, <Value3>
:SYSTem:TIME?
This command sets/gets the time of the clock built in the E4990A. When you logged in the E4990A as standard user, an error occurs.
|
Parameter |
Value1 |
|
Description |
hour |
|
Data Type |
Numeric type (Integer) |
|
Range |
0 to 23 |
|
Resolution |
1 |
|
Parameter |
Value2 |
|
Description |
Minute |
|
Data Type |
Numeric type (Integer) |
|
Range |
0 to 59 |
|
Resolution |
1 |
|
Parameter |
Value3 |
|
Description |
Second |
|
Data Type |
Numeric type (Integer) |
|
Range |
0 to 59 |
|
Resolution |
1 |
{numeric1(hour)}, {numerc2(minute)}, {numerc3(second)}<newline><^END>
Dim Var as Variant
Ana.WriteString ":SYST:TIME 10,10, 20", True
Ana.WriteString ":SYST:TIME?", True
Var=Ana.ReadList
System > Misc Setup > Clock Setup > Set Data and Time...
SCPI.SYSTEM.TIME