Setting up the Measurement

Other topics about Setting Measurement Conditions

Overview

The program listed in the below section is written in VISA-COM with Excel VBA. It can be executed from the external PC controller. The program demonstrates how to set up the measurement conditions.

Setting up Measurement Conditions Sample Program in Excel VBA

Sub Setup()

 '

    '

    ' The memory area of the resource manager and the instrument I/O are acquired

    Dim iomgr As VisaComLib.ResourceManager

    Dim Analyzer As VisaComLib.FormattedIO488

    

    Set iomgr = New VisaComLib.ResourceManager

    Set Analyzer = New VisaComLib.FormattedIO488

 

    ' Open the instrument. Sets the GPIB address.

    Set Analyzer.IO = iomgr.Open("USB0::0x0957::0x1809::KPR0200015::0::INSTR")

    ' TimeOut time should be greater than the measurement time.

    Analyzer.IO.timeout = 10000   

    '

    ' Initial Setup

    Analyzer.WriteString ":SYST:PRES", True

    ' Set two channel

    Analyzer.WriteString ":DISP:SPL D1_2", True

    ' Set trigger source at BUS.             

    Analyzer.WriteString ":TRIG:SOUR BUS", True                

    '

    ' Setup Channel 1

    ' Set measurement parameter for trace 1

    Analyzer.WriteString ":CALC1:PAR1:DEF Z", True

    ' Set measurement parameter for trace 2         

    Analyzer.WriteString ":CALC1:PAR2:DEF TZ", True

    ' Set Y-Axis at Log format         

    Analyzer.WriteString ":DISP:WIND1:TRAC1:Y:SPAC LOG", True   

 

    ' Stimulus Setup

    ' Turn on Continuous Activation mode for channel 1

    Analyzer.WriteString ":INIT1:CONT ON", True

    ' Set sweep type at LOG             

    Analyzer.WriteString ":SENS1:SWE:TYPE LOG", True

    ' Set number of point        

    Analyzer.WriteString ":SENS1:SWE:POIN 201", True

    ' Set start freqency       

    Analyzer.WriteString ":SENS1:FREQ:STAR 100E3", True

    ' Set stop frequency     

    Analyzer.WriteString ":SENS1:FREQ:STOP 10E6", True

   ' Set OSC mode       

    Analyzer.WriteString ":SOUR1:MODE VOLT", True

    ' Set OSC level           

    Analyzer.WriteString ":SOUR1:VOLT 300E-3", True

    ' Turn on ALC           

    Analyzer.WriteString ":SOUR1:ALC ON", True                  

    '

    ' Setup Channel 2

    ' Set measurement parameter for trace 1

    Analyzer.WriteString ":CALC2:PAR1:DEF CS", True

    ' Set measurement parameter for trace 2          

    Analyzer.WriteString ":CALC2:PAR2:DEF Q", True

    ' Split the trace windows           

    Analyzer.WriteString ":DISP:WIND2:SPL D1_2", True            

    

    ' Stimulus Setup

    ' Turn on Continuous Activation mode for channel 1

    Analyzer.WriteString ":INIT2:CONT ON", True

    ' Set sweep type at segment sweep            

    Analyzer.WriteString ":SENS2:SWE:TYPE SEGM", True

    ' Set segment dispay at freq base       

    Analyzer.WriteString ":DISP:WIND2:X:SPAC LIN", True        

    SegFmt = "7,0,1,0,0,0,0,0,3,"

    SegNo1 = "1E4,1E5,50,0,0.3," ' Start Freq, Stop Freq, Nop, Voltage Type, OSC level

    SegNo2 = "1E5,1E6,200,0,0.5,"

    segNo3 = "1E6,1E7,50,0,0.3"

    ' Set sweep type at LOG"

    Analyzer.WriteString ":SENS2:SEGM:DATA " & SegFmt & SegNo1 & SegNo2 & segNo3, True           

    '

    ' Save setting into state file

    ' Save settings to file

    Analyzer.WriteString ":MMEM:STOR ""D:\State\Test.sta""", True  

   

   ' Close IO

    Analyzer.IO.Close

        

End Sub