Using User Menu

Other topics about Using Macro

Overview

This sample program demonstrates the following operation.

  1. Set the softkey label of user menu (Macro Setup > User Menu).

  2. When user menu softkey is pressed, the Sub UserMenuButton_OnPress(bNo) is executed with the key number.

  3. The marker is operated according to the key number.

To use this sample:

  1. Copy the following code into a Notepad file.

  2. Save the file on the analyzer storage in the D: folder. Name the file as "userMenu.vbs".

  3. Double-click the file to execute.

Sample Program

dim ana

dim userMenu

dim bNo

dim mkrNo

set userMenu = WScript.CreateObject("E4990.UserMenu", "UserMenuButton_")

set ana = CreateObject("E4990.Application")

for bNo=1 to 5

   select case bNo

   case 1, 2, 3

   UserMenu.item(cint(bNo)).caption = "Marker" & bNo

   case 4

   UserMenu.item(cint(bNo)).caption = "Max"

   case 5

        UserMenu.item(cint(bNo)).caption = "Min"

   end select

next

Do Until False

    WScript.Sleep 500

Loop

Sub UserMenuButton_OnPress(bNo)

   Select case bNo

   

   case 1, 2, 3

        mkrNo=bNo

        ana.scpi.calculate.selected.marker(mkrNo).state = true

   ana.scpi.calculate.selected.marker(mkrNo).activate

   case 4

   ana.scpi.calculate.selected.marker(mkrNo).function.type ="maximum"

   ana.scpi.calculate.selected.marker(mkrNo).function.execute

   case 5

   ana.scpi.calculate.selected.marker(mkrNo).function.type ="minimum"

   ana.scpi.calculate.selected.marker(mkrNo).function.execute

   end select

End Sub