Command/Query
:CALCulate[:SELected]:FUNCtion:DOMain[:STATe] {ON|OFF|1|0}
:CALCulate[:SELected]:FUNCtion:DOMain[:STATe]?
This command sets/gets an arbitrary range for analysis.
When the trace coupling is OFF, the active trace is the target to be set.
|
Parameter |
Selection Option |
|
Description |
Analysis range On/Off status |
|
Data Type |
Boolean type (Boolean) |
|
Range |
ON|OFF|1|0 |
|
Preset Value |
OFF |
{1|0}<newline><^END>
Dim Var as Integer
Ana.WriteString ":CALC:FUNC:DOM ON", True
Ana.WriteString ":CALC:FUNC:DOM?", True
Var=Ana.ReadNumber
No equivalent key is available on the front panel.
SCPI.CALCULATE.SELECTED.FUNCTION.DOMAIN.STATE