:DISP:TABL:POS

Type

Query

Syntax

:DISPlay:TABLe:POSition[:RECTangle]?

Description

This command get/returns the rectangle position of list table.

Variable

Query Response

{numeric 1}, {numeric 2}, {numeric 3}, {numeric 4}<newline><^END>

Examples

Dim Var as Variant

Ana.WriteString ":DISP:TABL:POS?", True
Var=Ana.ReadNList

Related Commands

:DISP:TABL

:DISP:TABL:TYPE

Equivalent Softkey

No equivalent key is available on the front panel.

COM Command Syntax (Internal Control Only)

SCPI.DISPLAY.TABLE.POSITION.RECTANGLE