:DISP:WIND<Ch>:ACT

Type

Command

Syntax

:DISPlay:WINDow<Ch>:ACTivate

Description

This command specifies the active channel. You can set only a channel displayed to the active channel. If this object is used to set a channel not displayed to the active channel, an error occurs when executed and the object is ignored.

Examples

Ana.WriteString ":DISP:WIND:ACT", True

Related Commands

:DISP:WIND:SPL

Equivalent Softkey

Channel Prev, Channel Next

COM Command Syntax (Internal Control Only)

SCPI.DISPLAY.WINDOW(Ch).ACTIVATE