:HCOP:SDUM:DATA

Type

Query

Syntax

:HCOPy:SDUMp:DATA[:IMMediate]?

Description

This command allows to save the print screen image into an external PC.

Variable

Query Response

{byte}<newline><^END>

Examples

See Capturing Screen Into PC.

Related Commands

:HCOP:SDUM:DATA:FORM

Equivalent Softkey

No equivalent key is available on the front panel.

COM Command Syntax (Internal Control Only)

SCPI.HCOPY.SDUMP.DATA.IMMEDIATE