Query
*IDN?
This command reads the product information (manufacturer, model number, serial number, and firmware revision number) of the E4991B.
{string 1},{string 2},{string 3},{string 4}<newline><^END>
{string 1}: Manufacturer. "Keysight Technologies" is always read out.
{string 2}: Model number. "E4991B" is always read out.
{string 3}: Serial number (example: MY123400101).
{string 4}: Firmware revision number (example: A.01.00).
Dim Var as String
Ana.WriteString "*IDN?", True
Var=Ana.ReadString
System > Firmware Revision
SCPI.IEEE4882.IDN