Command/Query
*OPC
*OPC?
This command sets/gets the operation complete (OPC) bit (bit 0) of the Standard Event Status Register. When all of pending operations complete, *OPC returns 1.
{1}<newline><^END>
Dim Var as Integer
Ana.WriteString "*OPC?", True
Var=Ana.ReadNumber
No equivalent key is available on the front panel.
SCPI.IEEE4882.OPC