Command/Query
:INITiate<Ch>:CONTinuous {ON|OFF|1|0}
:INITiate<Ch>:CONTinuous?
This command turns ON/OFF the continuous initiation mode (setting by which the trigger system initiates continuously) in the trigger system.
|
Parameter |
Selection Option |
|
Description |
ON/OFF of the continuous initiation mode |
|
Data Type |
Boolean type (Boolean) |
|
Range |
ON|OFF|1|0 |
|
Preset Value |
OFF |
{1|0}<newline><^END>
Dim Var as Long
Ana.WriteString ":INIT1:CONT ON", True
Ana.WriteString ":INIT1:CONT?", True
Var=Ana.ReadNumber
Trigger > Hold | Continuous | Hold All Channels (This is not exact equivalent softkey.)
SCPI.INITIATE(Ch).CONTINUOUS