Command/Query
:MMEMory:TRANsfer <Value>
This command transfers data (file) between the built-in storage device of the E4991B and external PC through SCPI command, but not through COM command.
When you use directory names and file name, separate them with "/" (slash) or "\" (backslash). If a file with the specified file name already exists for writing or if the specified file does not exist for reading out (Query), an error occurs and the command is ignored.
|
Parameter |
Value |
|
Description |
File name on the built-in storage device |
|
Data Type |
Character string type (String) |
|
Range |
254 chars |
{Byte}<newline><^END>
See Transferring Files.
No equivalent key is available on the front panel.
SCPI.MMEMORY.TRANSFER