Command/Query
:SENSe<Ch>:CORRection<Type>:CKIT:OPEN:OFFSet <Value>
:SENSe<Ch>:CORRection<Type>:CKIT:OPEN:OFFSet?
This command sets/gets open offset value when measurement is set to either Impedance or Permeability measurement.
(<type>: User Calibration=1, Fixture Compensation=2)
|
Parameter |
Value |
|
Description |
Open offset value |
|
Data Type |
Numeric type (Real) |
|
Range |
-1M ~ 1M |
|
Preset Value |
0 |
|
Unit |
s |
|
Resolution |
- |
{numeric}<newline><^END>
Dim Var as Double, Var2 as String
Var= -1000000
Var2= "IMP"
Ana.WriteString ":SENS1:MODE " & Var2, True
Ana.WriteString ":SENS1:CORR:CKIT:OPEN:OFFS " & Str(Var), True
Ana.WriteString ":SENS1:CORR:CKIT:OPEN:OFFS?", True
Var=Ana.ReadNumber
Cal Compen > Calibration > Define Value > Open Offset Delay
Instrument Setup > Calibration > Define Value > Open Offset Delay
SCPI.SENSE(Ch).CORRECTION(Type).CKIT.OPEN.OFFSET