:SENS:ROSC:SOUR

Type

Query

Syntax

:SENSe:ROSCillator:SOURce?

Description

This command returns whether the external reference signal is inputted to the Ref In connector on the rear panel.

Query Response

{INT|EXT}<newline><^END>

INT: Internal
EXT: External reference signal is inputted

Examples

Dim Var as String
Ana.WriteString ":SENS:ROSC:SOUR?", True
Var=Ana.ReadString

Equivalent Softkey

Displayed on the instrument status bar (at the bottom of the LCD display).

COM Command Syntax (Internal Control Only)

SCPI.SENSE(Ch).ROSCILLATOR.SOURCE