Command/Query
:TRIGger[:SEQuence]:EXTernal:DELay <Value>
:TRIGger[:SEQuence]:EXTernal:DELay?
This command sets/gets the time that it takes from receiving the trigger to starting measurement when the trigger source is external.
|
Parameter |
Value |
|
Description |
External trigger delay time |
|
Data Type |
Numeric type (Real) |
|
Range |
0 to 10 |
|
Preset Value |
0 |
|
Unit |
s |
|
Resolution |
10u |
{0 ~ 10}<newline><^END>
Dim Var as Double
Var= 0
Ana.WriteString ":TRIG:EXT:DEL" & Str(Var), True
Ana.WriteString ":TRIG:EXT:DEL?", True
Var=Ana.ReadNumber
Trigger > Trigger Delay
SCPI.TRIGGER.SEQUENCE.EXTERNAL.DELAY