The method of connecting the DUT (1608 (mm) / 0603 (inch) size) to the 16197A is described as an example.
Push the latch button while pressing the lever to set the DUT connection terminal of the test fixture to the OPEN state.
Remove the short device.
Place the DUT in the same way as you placed the short device, as shown below.

Release the latch button while pressing the lever and then release the lever slowly.