User Account and Password

Other topics about Using Windows

Account Settings

The E4991B measurement application can be executed with both administrator and standard user type of account with windows.

The below account settings are available:

User Name

Password

Type

Description

Instrument

measure4u (Windows 7 and Windows 10 with storage revision BF2xx and below)

Keysight4u! (Windows 11/ Windows 10 with storage revision BG30x and above.)

Administrator

Auto Log On is activated by default.

Administrator

agielnt4u (Windows 7)

keysight4u (Windows 10 with storage revision BF2xx and below / Windows 7 with storage revision KB100 and above)

Keysight4u! (Windows 11/ Windows 10 with storage revision BG30x and above.)

Built-in Administrator

For user maintenance purpose.

To be determined by user

To be determined by user

Administrator or Standard user

Not a default account setting. However, can be added by user.

Keysightonly

Not disclosed to user

Administrator

This account is used by Keysight Service in case of repair/maintenance.

  • Do not remove this account.

Standard User Limitation

The standard user account has some limitation in access, especially in performing the below tasks. These are only allowed with administrator account:

User Account Control

With administrator account, you are allowed to modify the User Account Control settings. To access the User Account Control setting, open Control Panel, click on User Accounts > Change User Account Control settings. The default setting is Notify me only when programs try to make changes to my computer.  With this selection, you are notified each time a program tries to make any changes to your computer. Other available settings are not guaranteed in the E4991B operation.

With a standard user account, default setting (Notify me only when programs try to make changes to my computer) should be selected before you leave from an administrator account.

To Change Password

You are allowed to change an account's password.

Change Password

  1. Open User Accounts in Control Panel.

  2. Click Add or remove user accounts.

  3. Click on the account you would like to change password from the Choose the account you would like to change.

  4. Click Change the password.

  5. Enter new password, confirm new password and password hint.

  6. Click Change Password button.

To Add and Remove User

Adding new user and removing existing user can be done via Control Panel.

Add New User

  1. Open User Accounts in Control Panel.

  2. Click Add or remove user accounts.

  3. Click Create a new account.

  4. Enter the new account name.

  5. Select either Standard user or Administrator.

  6. Click Create Account button.

  7. The administrator authority is necessary for some of function in E4991B. Select computer administrator when you make the user account.

Remove Existing User

  1. Open User Accounts in Control Panel.

  2. Click Add or remove user accounts.

  3. Click on the account you would like to remove from the Choose the account you would like to change.

  4. Click Delete the account.

  5. Window message confirming if you would like to keep or delete the account's files prompts.

  6. Click either Delete Files or Keep Files button.

  7. Next windows message prompts seeking confirmation if you are sure of deleting the selected account.

  8. Click on Delete Account button.