If files saved with the standard model contain data trace, “state & data”, having not-allowed parameters such as start offset frequency down to 1 Hz, they cannot be recalled with the option 011. In case that files contain instrument settings only, “state only”, which is not available for the option 011, that parameters is automatically set to the initial settings of the option 011.