Protecting SSA System

To protect your SSA, follow the instructions below:

  1. Read the warning labels and specifications

Do not exceed the values provided in the specifications guide or as indicated by the yellow warning labels on the front panel of SSA. Refer to the specifications for the conditions required to meet the listed specifications. There will be information regarding SSA settings.

  1. Do NOT Plug off Power Cable during Shutdown Process

If you directly interrupt the power supply to the power cable receptacle when the power supply is on, or turn off the Line Switch (Always ON), the shutdown process will not work. This could damage the HDD of the E5052B.

  1. Do NOT Modify or Reconfigure the Operating System

The Microsoft Windows operating system has been modified and optimized by Keysight to improve the performance of the SSA.

  1. Install Antivirus Protection

The SSA does NOT have antivirus protection when shipped. Use of an antivirus program is strongly recommended if you connect the SSA to the LAN (Internet).

In addition, the use of a firewall could help to protect the SSA from viruses. However, some firewalls could limit DCOM connectivity of the SSA.

  1. Install Windows Critical Updates

The SSA is always shipped with the latest service packs and critical updates that were available at the time that the SSA is produced. We recommend that you maintain the latest available protection for your SSA by automatically accepting and installing the latest critical security patches from the Microsoft Windows Update website: http://windowsupdate.microsoft.com

  1. Run Error Check and Disk Defragmenter

When the SSA is shutdown unexpectedly or power is removed without first shutting down, large amounts of Hard Disk Drive space is rendered unusable. If shutdown in this manner enough times, the SSA could become unstable and no longer work.

This HDD space can be recovered by first running Windows Error-checking to find and correct errors on the disk, and then the Disk Defragmenter to recover Hard Disk Drive space. See the Windows Help file for more information about Disk Defragmenter.

  1. Precaution for Use of Hard Disk

Do NOT Modify or delete any Files and Folders in Drive other than D and E: Drive.(These two drives, D and E are available to use as Data backup). Doing so will result in malfunctioning of the device. It is required to execute the System recovery if there are any troubles with the above operations.

  1. Precaution for RF input connector and cable

  1. Precautions for Electrostatic Discharge (ESD)

ESD can damage or destroy electronic components. Whenever possible, conduct testing at a static-safe workstation. Keep static-generating materials at least one meter away from all components. Before connecting any coaxial cable to an analyzer, momentarily short the center and outer conductors of the cable together.

  1. Maintain working environment condition

Control your environment. Maintain temperature & humidity with a satisfactory range within the instruments specification and prevent large fluctuations.

  1. Precautions for transportation

  1. Check for Proper Ventilation

Periodically check and clean the cooling vents of the SSA. Inadequate airflow can result in excessive operating temperatures  which can lead to instrument failures. When installing the product in a cabinet, the convection into and out of the instrument must not be restricted. The ambient temperature must be less then the maximum operating temperature of the product by 4°C for every 100 watts dissipated in the cabinet. If the total power dissipated in the cabinet is greater than 800 watts, then forced convection must be used.

  1. Precautions for Proper Grounding