A warning message is displayed in the instrument message/Warning area in the lower-left part of the display against a gray background. Touching Entry Off key at the front panel executing the :DISPlay:MESSage:CLEar command clears the message. Moreover, about a specific warning message, when a sweep is started again, a warning message may disappear.
This message simply appears on the display, since it is not known to remote environments such as a GPIB. This message is not displayed when another error message (against a red background) has already been displayed in the instrument message/Warning area.
The warning messages for this instrument are as follows:
|
No. |
Message |
Description |
|
571 |
DC control out of limit |
This message occurs when the specified DC control voltage or the sweep start/stop DC control voltage for the frequency & power measurement is out of the maximum/minimum allowed voltage of DC control. |
|
580 |
DC control output ON required in AFC |
The automatic frequency control function was set on, however, the power or control voltage is not being applied to the DUT. Verify that the control voltage output is set to ON. |
|
570 |
DC power out of limit |
This message occurs when the specified DC power voltage or the sweep start/stop DC power voltage for the frequency & power measurement is out of the maximum/minimum allowance voltage of DC control. |
|
560 |
Incompatible recall file |
This message occurs when an incompatible file is read. |
|
550 |
Marker tracking failed |
This message occurs when marker tracking fails. |
|
503 |
Set RF ATT 0dB |
This message occurs when the input attenuator is set improperly. Set the input attenuator to 0 dB .
|
|
504 |
Set RF ATT 5dB |
This message occurs when the input attenuator is set improperly. Set the input attenuator to 5 dB. |
|
505 |
Set RF ATT 10dB |
This message occurs when the input attenuator is set improperly. Set the input attenuator to 10 dB. |
|
506 |
Set RF ATT 15dB |
This message occurs when the input attenuator is set improperly. Set the input attenuator to 15 dB. |
|
507 |
Set RF ATT 20dB |
This message occurs when the input attenuator is set improperly. Set the input attenuator to 20 dB. |
|
508 |
Set RF ATT 25dB |
This message occurs when the input attenuator is set improperly. Set the input attenuator to 25 dB. |
|
510 |
Set RF ATT 30dB |
This message occurs when the input attenuator is set improperly. Set the input attenuator to 30 dB. |
|
511 |
Set RF ATT 35dB |
This message occurs when the input attenuator is set improperly. Set the input attenuator to 35 dB. |
|
590 |
Unable to find help file |
Help file doesn't appear |
|
591 |
Failed to read help file |
Help file is found. But could not be read.
|
|
561 |
Recall in bad condition |
This message occurs when the measurement data does not corresponds with the X-axis value of the reading data. |