By executing system recovery, you can return the system of the E5052B (the Windows operating system and the firmware) to the factory state (at the time of purchase) or the user state at the setting the user performed save user state.
User state recovery function is available at HDD revision NM320 and below.
The procedure of system recovery is described in both installation manual and Service Manual.
Other topics about Maintenance