SCPI.CALCulate.AM(Ch).TRACe(Tr).LIMit.LOWer.LDATa

Object Type

Property (Read-Write)

Syntax

SCPI.CALCulate.AM(Ch).TRACe(Tr).LIMit.LOWer.LDATa = Value

Value = SCPI.CALCulate.AM(Ch).TRACe(Tr).LIMit.LOWer.LDATa

Description

This command sets/gets expanded lower limit line, for the selected trace Tr of the selected channel Ch.

Variable

Parameter

   Value

Description

Lower limit line

Data Type

Variant type Array (Range)

Range

1...1601

Preset Value

-

Unit

-

Resolution

-

Preset Effect

No

Save-Recall Effect

No

Error

-

Examples

Dim Var(1 to 1601) as Variant
SCPI.CALCulate.AM1.TRACe1.LIMit.LOWer.LDATa = Var
Var = SCPI.CALCulate.AM1.TRACe1.LIMit.LOWer.LDATa

Related Objects

SCPI.CALCulate.AM(Ch).TRACe(Tr).LIMit.FAIL

SCPI.CALCulate.AM(Ch).TRACe(Tr).LIMit.LOWer.SEGMent.CLEar

SCPI.CALCulate.AM(Ch).TRACe(Tr).LIMit.LOWer.SEGMent.COUNt

SCPI.CALCulate.AM(Ch).TRACe(Tr).LIMit.LOWer.SEGMent.DATA

SCPI.CALCulate.AM(Ch).TRACe(Tr).LIMit.REPort.DATA

SCPI.CALCulate.AM(Ch).TRACe(Tr).LIMit.STATe

SCPI.CALCulate.AM(Ch).TRACe(Tr).LIMit.UPPer.LDATa

SCPI.CALCulate.AM(Ch).TRACe(Tr).LIMit.UPPer.SEGMent.CLEar

SCPI.CALCulate.AM(Ch).TRACe(Tr).LIMit.UPPer.SEGMent.COUNt

SCPI.CALCulate.AM(Ch).TRACe(Tr).LIMit.UPPer.SEGMent.DATA

Equivalent Key

No equivalent key is available on the front panel.

Equivalent SCPI Command

Syntax

:CALCulate:AM[1-1]:TRACe[1-1]:LIMit:LOWer:LDATa {1...1601}

:CALCulate:AM[1-1]:TRACe[1-1]:LIMit:LOWer:LDATa?

Query Response

{1...1601} <newline><^END>

Example of use

10 Dim A(1:1601)
20 OUTPUT 717;":CALCulate:AM1:TRACe1:LIMit:LOWer:LDATa 1,1601"
30 OUTPUT 717;":CALCulate:AM1:TRACe1:LIMit:LOWer:LDATa ?"
40 ENTER 717;A(*)