SCPI.CALCulate.BB(Ch).TRACe(Tr).FORMat

Object Type

Property (Read-Write)

Syntax

SCPI.CALCulate.BB(Ch).TRACe(Tr).FORMat = Value

Value = SCPI.CALCulate.BB(Ch).TRACe(Tr).FORMat

Description

This command sets/gets BB format, for the selected trace Tr of the selected channel Ch.

Variable

Parameter

   Value

Description

BB format

Data Type

Character string type (String)

Range

DBVHz|DBMHz|VHz

Preset Value

DBVHz

Unit

-

Resolution

-

Preset Effect

Yes

Save-Recall Effect

Yes

Error

-

Examples

Dim Var as String
Var= "DBVHz"
SCPI.CALCulate.BB1.TRACe1.FORMat = Var
Var = SCPI.CALCulate.BB1.TRACe1.FORMat

Equivalent Key

BB Menu: Format > Format

Equivalent SCPI Command

Syntax

:CALCulate:BB[1-1]:TRACe[1-1]:FORMat {DBVHz|DBMHz|VHz}

:CALCulate:BB[1-1]:TRACe[1-1]:FORMat?

Query Response

{DBVHz|DBMHz|VHz} <newline><^END>

Example of use

10 OUTPUT 717;":CALCulate:BB1:TRACe1:FORMat DBVHz"
20 OUTPUT 717;":CALCulate:BB1:TRACe1:FORMat ?"
30 ENTER 717;A$