SCPI.CALCulate.FP(Ch).DATA.RDATa

Object Type

Property (Read-Write)

Syntax

SCPI.CALCulate.FP(Ch).DATA.RDATa = Value

Value = SCPI.CALCulate.FP(Ch).DATA.RDATa

Description

This command sets/gets measurement raw data, for the selected channel Ch.

Variable

Parameter

   Value

Description

Measurement raw power data

Data Type

Variant type Array (Range)

Range

1...3003

Preset Value

-

Unit

-

Resolution

-

Preset Effect

No

Save-Recall Effect

No

Error

-

Examples

Dim Var(1 to 3003) as Variant
SCPI.CALCulate.FP1.DATA.RDATa = Var
Var = SCPI.CALCulate.FP1.DATA.RDATa

Related Objects

SCPI.CALCulate.FP(Ch).DATA.TDATa

SCPI.CALCulate.FP(Ch).DATA.XDATa

Equivalent Key

No equivalent key is available on the front panel.

Equivalent SCPI Command

Syntax

:CALCulate:FP[1-1]:DATA:RDATa {1...3003}

:CALCulate:FP[1-1]:DATA:RDATa?

Query Response

{1...3003} <newline><^END>

Example of use

10 Dim A(1:3003)
20 OUTPUT 717;":CALCulate:FP1:DATA:RDATa 1,3003"
30 OUTPUT 717;":CALCulate:FP1:DATA:RDATa ?"
40 ENTER 717;A(*)