Property (Read-Write)
SCPI.CALCulate.SP(Ch).TRACe(Tr).FORMat = Value
Value = SCPI.CALCulate.SP(Ch).TRACe(Tr).FORMat
This command sets/gets SP format, for the selected trace Tr of the selected channel Ch.
|
Parameter |
Value |
|
Description |
SP format |
|
Data Type |
Character string type (String) |
|
Range |
DBM|DBV|WATT|VOLT|DBMHz|DBVHz|WHZ|VHZ |
|
Preset Value |
DBM |
|
Unit |
- |
|
Resolution |
- |
|
Preset Effect |
Yes |
|
Save-Recall Effect |
Yes |
|
Error |
- |
Dim Var as String
Var= "DBM"
SCPI.CALCulate.SP1.TRACe1.FORMat = Var
Var = SCPI.CALCulate.SP1.TRACe1.FORMat
SP Menu: Format > Format
:CALCulate:SP[1-1]:TRACe[1-1]:FORMat {DBM|DBV|WATT|VOLT|DBMHz|DBVHz|WHZ|VHZ}
:CALCulate:SP[1-1]:TRACe[1-1]:FORMat?
{DBM|DBV|WATT|VOLT|DBMHz|DBVHz|WHZ|VHZ} <newline><^END>
10 OUTPUT 717;":CALCulate:SP1:TRACe1:FORMat DBM"
20 OUTPUT 717;":CALCulate:SP1:TRACe1:FORMat ?"
30 ENTER 717;A$