Property (Read-Write)
SCPI.CALCulate.TR(Ch).TRACe(Tr).REFerence.FREQuency = Value
Value = SCPI.CALCulate.TR(Ch).TRACe(Tr).REFerence.FREQuency
This command sets/gets frequency reference for DHZ, PCT, PPM, for the selected trace Tr of the selected channel Ch.
|
Parameter |
Value |
|
Description |
Frequency reference for DHZ, PCT & PPM |
|
Data Type |
Double precision floating point type (Double) |
|
Range |
-500G ~ 500G |
|
Preset Value |
0 |
|
Unit |
Hz |
|
Resolution |
- |
|
Preset Effect |
Yes |
|
Save-Recall Effect |
Yes |
|
Error |
- |
Dim Var as Double
Var= -500000000000
SCPI.CALCulate.TR1.TRACe4.REFerence.FREQuency = Var
Var = SCPI.CALCulate.TR1.TRACe4.REFerence.FREQuency
TR Menu: Format > Frequency Reference
TR Menu: Format > Marker > Frequency Reference
:CALCulate:TR[1-1]:TRACe[1-8]:REFerence:FREQuency {-500G ~ 500G}
:CALCulate:TR[1-1]:TRACe[1-8]:REFerence:FREQuency?
{-500G ~ 500G} <newline><^END>
10 OUTPUT 717;":CALCulate:TR1:TRACe4:REFerence:FREQuency -500000000000"
20 OUTPUT 717;":CALCulate:TR1:TRACe4:REFerence:FREQuency ?"
30 ENTER 717;A