Property (Read-Write)
SCPI.CONTrol.HANDler.D.MODE = Value
Value = SCPI.CONTrol.HANDler.D.MODE
This command sets/gets direction of port D.
|
Parameter |
Value |
|
Description |
Direction of Port D |
|
Data Type |
Character string type (String) |
|
Range |
INPut|OUTPut |
|
Preset Value |
INPut |
|
Unit |
- |
|
Resolution |
- |
|
Preset Effect |
No |
|
Save-Recall Effect |
No |
|
Error |
- |
Dim Var as String
Var= "INPut"
SCPI.CONTrol.HANDler.D.MODE = Var
Var = SCPI.CONTrol.HANDler.D.MODE
No equivalent key is available on the front panel.
:CONTrol:HANDler:D:MODE {INPut|OUTPut}
:CONTrol:HANDler:D:MODE?
{INPut|OUTPut} <newline><^END>
10 OUTPUT 717;":CONTrol:HANDler:D:MODE INPut"
20 OUTPUT 717;":CONTrol:HANDler:D:MODE ?"
30 ENTER 717;A$