SCPI.DISPlay.BB(Ch).TRACe(Tr).X.SCALe.RIGHt

Object Type

Property (Read-Write)

Syntax

SCPI.DISPlay.BB(Ch).TRACe(Tr).X.SCALe.RIGHt = Value

Value = SCPI.DISPlay.BB(Ch).TRACe(Tr).X.SCALe.RIGHt

Description

This command sets/gets right setting for X axis, for the selected trace Tr of the selected channel Ch.

Variable

Parameter

   Value

Description

Right setting for X axis

Data Type

Double precision floating point type (Double)

Range

1.1 ~ 100M

Preset Value

10M

Unit

-

Resolution

-

Preset Effect

Yes

Save-Recall Effect

Yes

Error

-

Examples

Dim Var as Double
Var= 0
SCPI.DISPlay.BB1.TRACe1.X.SCALe.RIGHt = Var
Var = SCPI.DISPlay.BB1.TRACe1.X.SCALe.RIGHt

Related Objects

SCPI.DISPlay.BB(Ch).TRACe(Tr).X.SCALe.AUTO

SCPI.DISPlay.BB(Ch).TRACe(Tr).X.SCALe.LEFT

Equivalent Key

BB Menu: Scale > X Axis > Right

Equivalent SCPI Command

Syntax

:DISPlay:BB[1-1]:TRACe[1-1]:X[:SCALe]:RIGHt {1.1 ~ 100M}

:DISPlay:BB[1-1]:TRACe[1-1]:X[:SCALe]:RIGHt?

Query Response

{1.1 ~ 100M} <newline><^END>

Example of use

10 OUTPUT 717;":DISPlay:BB1:TRACe1:X[:SCALe]:RIGHt 0"
20 OUTPUT 717;":DISPlay:BB1:TRACe1:X[:SCALe]:RIGHt ?"
30 ENTER 717;A