SCPI.DISPlay.FP(Ch).ALLTrace.PERSistence.CLEar

Object Type

Method (Write Only)

Syntax

SCPI.DISPlay.FP(Ch).ALLTrace.PERSistence.CLEar

Description

This command clears all stored traces, for the selected channel Ch.

Examples

SCPI.DISPlay.FP1.ALLTrace.PERSistence.CLEar

Equivalent Key

No equivalent key is available on the front panel.

Equivalent SCPI Command

Syntax

:DISPlay:FP[1-1]:ALLTrace:PERSistence:CLEar

Example of use

10 OUTPUT 717;":DISPlay:FP1:ALLTrace:PERSistence:CLEar"