Property (Read-Write)
SCPI.DISPlay.TR(Ch).PARameter = Value
Value = SCPI.DISPlay.TR(Ch).PARameter
This command sets/gets window setting, for the selected channel Ch.
This function is available when measurement mode is Narrow/Narrow.
|
Parameter |
Value |
|
Description |
Window setting |
|
Data Type |
Character string type (String) |
|
Range |
ALL|FREQuency|POWer|PHASe |
|
Preset Value |
ALL |
|
Unit |
- |
|
Resolution |
- |
|
Preset Effect |
Yes |
|
Save-Recall Effect |
Yes |
|
Error |
- |
Dim Var as String
Var= "FREQuency"
SCPI.SENSe.TR1.MMODe = "NN"
SCPI.DISPlay.TR1.PARameter = Var
Var = SCPI.DISPlay.TR1.PARameter
TR Menu: Display > Parameters
:DISPlay:TR[1-1]:PARameter {ALL|FREQuency|POWer|PHASe}
:DISPlay:TR[1-1]:PARameter?
{ALL|FREQuency|POWer|PHASe} <newline><^END>
10 OUTPUT 717;":SENSe:TR1:MMODe NN"
20 OUTPUT 717;":DISPlay:TR1:PARameter FREQuency"
30 OUTPUT 717;":DISPlay:TR1:PARameter?"
40 ENTER 717;A$