Property (Read-Write)
SCPI.DISPlay.USER(Ch).TRACe(Tr).STATe = Value
Value = SCPI.DISPlay.USER(Ch).TRACe(Tr).STATe
This command sets/gets trace state i.e. enable/disable. At least one trace must be turned on., for the selected trace Tr of the selected channel Ch.
|
Parameter |
Value |
|
Description |
Trace state |
|
Data Type |
Boolean type (Boolean) |
|
Range |
ON|OFF|1|0 |
|
Preset Value |
ON |
|
Unit |
- |
|
Resolution |
- |
|
Preset Effect |
Yes |
|
Save-Recall Effect |
Yes |
|
Error |
61, "Failed to hide trace" |
Dim Var as Boolean
Var= 1
SCPI.DISPlay.USER1.TRACe8.STATe = Var
Var = SCPI.DISPlay.USER1.TRACe8.STATe
USER Menu: Trace View > Enable Trace > Trace 1
:DISPlay:USER[1-1]:TRACe[1-8]:STATe {ON|OFF|1|0}
:DISPlay:USER[1-1]:TRACe[1-8]:STATe?
{ON|OFF|1|0} <newline><^END>
10 OUTPUT 717;":DISPlay:USER1:TRACe8:STATe 1"
20 OUTPUT 717;":DISPlay:USER1:TRACe8:STATe ?"
30 ENTER 717;A